Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

MediaService Digital Industries Newsroom

The MediaService Digital Industries: a publication designed to bring you the latest and most interesting news and features on all kinds of industry-related features under the topic headings Automation Technology, Industrial Software, Communications and Services as also Market-Specific Solutions (e.g. Automotive, Aerospace, Chemicals, Food and Beverages, Pharmaceuticals, Machine Building).
MediaService application reports may be based on previously published Siemens technical articles.

Receive regular news and up-to-date information about Digital Industries solutions

Digithek for downloading individual articles from all the MediaService Digital Industries issues

Current online article

03. August 2020                                                                                                      
Extended functionality  Firmware update for Simatic RF100C communication modules

Siemens is expanding its portfolio for industrial communication networks. With the IE/PB Link HA gateway, which is optimized for use in the process industry, highly redundant infrastructures can be implemented based on the open Profinet Industrial Ethernet standard. This ensures uninterrupted system operation, not least because changes can be made to the configuration during ongoing operation. In addition, the gateway is suitable for use in harsh ambient conditions and temperatures from -40 to +70 degrees Celsius. 
Read the article

Further online articles

27. July 2020                                                                                                      
Extended functionality  Firmware update for Simatic RF100C communication modules

Siemens is now providing the firmware V1.3 with extended functions for the new generation Simatic RF100C communication modules. The Ethernet/IP and XML protocols are now available for all Ethernet-based modules, and the Profibus module now also supports the Simatic RF600 series readers. Additional readers and devices can also be operated on all communication modules via the Freeport setting.
Read the article

20. July 2020                                                                                                      
Staying on track – Siemens components significantly optimize truck tire test bench performance

The French tire manufacturer Michelin operates a truck tire test bench at its Ladoux site. As part of its modernization program, Michelin now relies on Siemens automation components which have replaced the existing system. Not only does the new solution provide measurements which are compatible with the existing system, but the new technology is also several times more accurate than the previous model. In addition to this, Michelin now benefits from high data consistency and repeatability.
Read the article

Online Articles September 2019

Online Articles August 2019

Contact

Ursula Lang

MediaService

+49 (152) 22915052

Andreas Friedrich

Factory Automation (Products & Innovations)

+49 (1522) 2103967

Julia Kauppert

Industry Branches

+49 (174) 3118098

Katharina Lamsa

Motion Control

+49 (172) 8413539

Katharina Zoefeld

Process Automation

+49 (172) 5876725

Evelyne Kadel

Process Automation

+49 (173) 5649708

David Petry

Communication Networks, MindSphere, Services

+49 (173) 5371050

Claudia Lanzinger

Software

+49 (160) 90450 431

Sabine Schindler

Technical Articles

+49 (152) 214 50728

Stefan Rauscher

Large Drives Applications

+49 (152) 22805502